Where can I get Seismic Qualification Documentation on the Altivar Process?
Issue:
Seismic Qualification Documentation on the Altivar Process

Product Line:
Altivar Process Drive

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
There is no seismic document for Altivar Process. No test has been performed for this.
However each drive's product datasheet does provide information on vibration and shock resistance.  See example below

For instance, with an ATV630D11N4:
Vibration Resistance:
1 gn (f = 13...200 Hz) conforming to EN/IEC 60068-2-6
1.5 mm (f = 3...13 Hz) conforming to EN/IEC 60068-2-6
Shock Resistance:
15 gn for 11 ms conforming to IEC 60068-2-27

These values are available in the datasheet of the product (http://eshop.schneider-electric.com/product.aspx?org=21&lang=1&dist=276&prod_id=ATV630D11N4).

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj