What are the possible causes and remedies for Err4 on ATV212 Drives?
Issue:
Causes and remedies for Err4 on ATV212.

Product Line:
ATV212, ATV21, S-Flex

Resolution:
It is a Main Control Board CPU Error. The Control Board CPU is inoperable. Disconnect Control wire(s) from P24 and PP terminals. Cycle power to the drive.

If problem persists, try to reset the drive using tyP parameter. If VFD will not allow any parameter change then replace the VFD.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj