Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
How to do program the ATV630 for 2- wire control and where do I connect the start / stop?
Issue:
Program the ATV630 for 2-wire control and connect the start / stop.

Product Line:
ALTIVAR 630

Environment:
All serial numbers

Cause:
Installation / Setup

Resolution:
Go to menu 5 Complete Settings
Go to menu 5.5 Command and Reference
Set 2/3 wire type to 2 wire .
​24V to DI1 = forward (normally open , maintained close to start)