How to write a script that creates a form with radio buttons
DISCLAIMER

The example below is intended to demonstrate one or more features or methods and is presented as a configuration example only. Schneider Electric assumes no liability for the use or application of this example or any portion thereof.


Attached there is an example script showing how to create a customized form with radio buttons.
You can import the SDE file to ClearSCADA 2015 R1 or newer. It will create a folder called "Radio button script". The script itself is in the "Default" mimic inside that folder and is triggered by the "Test" button:





Please read the script comments for more details.

Schneider Electric Sverige

Bilagor
Radio Button Script.sde [563.67 KB]