Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Can ATV320 be powered by DC bus using Bonitron unit?
Issue:
Can I use Bonitron unit connected on the DC bus to power up the ATV320 drive?

Product Line:
ATV320, Altivar 320

Environment:
All

Cause:
Customer has 1-phase line power.

Resolution:
Technically, if the Bonitron unit is sized properly, it could work. However, We have not tested that combination, and we have no UL listing on it.