Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What IP address does M580 DHCP server use?
Issue

Customers are often confused whether which M580 IP address (main IP or IP A) is used as DHCP server IP address.

Product Line

M580


Resolution

The DHCP server uses the main IP of the CPU to serve the CRA as well as the X80 HART modules.