Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Which cable is used to connect from an RJ-45 based RS-232 port on the SCADAPack controller to DE-9P connector on PC?
Schneider Electric 3-wire serial cable p/n TBUM297217 is used to connect from an RJ-45 based RS-232 port on the SCADAPack 32 controller to DE-9P connector on a DTE such as a PC.