Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
How to configure 8SW switch output module for low battery status?
The 8SW switch output module provides eight switch closures and can be configured to open and close based on the process value value or status of a field unit.
1. Connect PC to the Base radio and 8SW switch output module via RS485 communications.
2. Open Accutech Manager and logon.
3. Select Base & Output Devices.
4. Double click on the Analog/Digital Output module and a Output device properties window will appear.
5. Select Switch1 and configure to Monitor Field unit Status then enable the Low Battery to monitor conditions.
Accutech Manager