Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Can plugging and unplugging of Ethernet cables from ports of BMENOC0301 and BMENOC0311 module can generate events which are logged in syslog server.
Yes it is possible to log the following events from BMENOC0301 and BMENOC0311 module to syslog server

1. Ethernet port link status
2. RSTP Topology change
3. FTP Login successful or denied
4. TCP Connection denied due to Access Control List
5. ENOCs Start, Stop, Run