What is the weight capacity of NetShelter open frame racks: AR201, AR203A and AR204A?
Issue:
Static load rating is required.

Product Line:
NetShelter Open Frame Racks

Environment:
All models, all serial numbers.

Cause:
On the APC website, weight capacity is not noted in the Specifications tab of the product pages.

Resolution:
AR203A and AR204A Weight Capacity 2,000 lb (907.18 kg).
AR201 Weight Capacity 1,000 lb. (453.6 kg).

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj