Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Why am I being prompted for a Password when attempting to upgrade BMENOC0301 firmware?
Issue
When trying to flash firmware to the NOC module with Unity Loader 10 or higher a password is requested.

Product line
Unity Loader, BMENOC0301

Resolution
As of Unity Loader v10 the ability to set a password for firmware downloads was activated.

Use the password fwdownload as this is the default password for the firmware download.