Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Can I add a communication option card to an "E" version of the ATV340 series drives?
Issue:
Add a communication option card to an "E" version of the ATV340.

Product Line:
ATV340 series drives.

Environment:
All models ending with "E", All serial numbers.

Cause:
Clarification of available options.

Resolution:
The "E" version of the ATV340 series drive has embedded Ethernet communication.  Additional communication options can not be added to this version of the drive.  If communication options other than Ethernet are needed for the ATV340 series drive, a non-Ethernet version (no E at the end of part number) ATV340 series drive will be needed.