Which RS-232 cable is used for communication from PC to SCADAPack 4000 series Transmitters?
Schneider Electric 3-wire serial cable p/n TBUM297801 is used to connect from an 3-pin based RS-232 port on the SCADAPack 4000 series Transmitter (4012, 4032, 4102, 4203DR, 4203DS) to DE-9P connector on a DTE such as a PC.