Can the Process Drive keypad be removed from the drive?
Issue:
Can the Process Drive keypad be removed from the drive?

Product Line:
Altivar Machines, Altivar 630, Altivar 930
Environment:
All

Cause:
Customer wants to remove the keypad

Resolution:
Yes, the keypad (HMI) can be removed from Process Drives, unless you are controlling the drive with the keypad it will have a fault / drive will stop when keypad is removed.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj