Våra varumärken

Impact-Company-Logo-English Black-01-177x54

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
If a customer needs to locally source the 5mm hole plugs used on NetShelter SX frames (827-0022), do we have manufacturer part numbers to reference?
Issue:
A customer wants to source 5mm black hole plugs locally.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
The hole plugs may have been removed and lost.

Resolution:


Fastenal #99882424
ITW Fastex 254-120601-00-2099