Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Is there a way to increase the number of backplane transactions serviced by the CPU per mast cycle
Issue
Is there a way to increase the number of backplane transactions serviced by the CPU per mast cycle

Product Line
M580

Environment
Unity, Control Expert.

Resolution
Yes.  %SW90 allows the user to control the number of backplane transactions serviced by the CPU per mast cycle