Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What can cause an INF7 [Internal Error 7] on an ATV340 series drive and how do I correct it?
Issue:
Customer is experiencing an INF7 [Internal Error 7] on an ATV340 series drive.

Product Line:
Altivar Machines, Altivar 340

Environment:
All models and serial numbers

Cause:
Communication interruption with CPLD component of Control Board.

Resolution:
Contact our local Schneider Electric representative.