NO, During the Scadapack 300 series RTU Sleep mode, the 5Vdc power to the I/O bus is switched off. Therefore, no I/O expansion module will be operating.The other option is used the the 3 counter inputs on the controller board because it will continue to function while its on sleep mode.
Publicerad för: Schneider Electric Sverige