SBO server communication on different TCP ports
Testing installation:
ES software administrator
HTTP: 80, HTTPS: 443, TCP: 5555
ES Workstation: Communication tab
ES <ip.addr.> TCP port 5555 <editable>
AS <ip.addr.> TCP port 4444 <editable>
AS Workstation: Communication tab
ES <ip.addr.> TCP port 5555 <editable>
AS <ip.addr.> TCP port 4444 <read only>

COMMUNICATION:
Type 1
Enterprise server                                                  AS-P
58563 <--------------------- PSH ACK ------------------------ 4444
58563 ---------------------- PSH ACK -----------------------> 4444
58563 <---------------------    ACK     ------------------------ 4444
58563 ----------------------     ACK     -----------------------> 4444
Type 2
Enterprise server                                                  AS-P
5555 <--------------------- PSH ACK ------------------------ 54465
5555 ---------------------- PSH ACK -----------------------> 54465
5555 <---------------------    ACK     ------------------------ 54465
5555 ----------------------     ACK     -----------------------> 54465

Both type are used during communication.
It depends on type of information which is transfered.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj