Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
AltivarProcess ATV600, ATV900 Variable speed drive: Identifying Active Configuration in Multi-Configuration or Multi-Motor Setup in the PLC code
To know which configuration is active, read register CNFS (active configuration) at address 8020.
Values returned:
0 = in progress (during changing configuration)
1= config 0 is active
2=config 1 is active
3=config 2 is active
4=config 3 is active