The following article describes the steps necessary to configure a DNP3 Generic Direct Outstation over TCP in ClearSCADA as follows:
1- Create a DNP3 Direct Channel- right-click where you want to create the channel select DNP3 and select Direct Channel.
2- Configure the Direct Channel as follows:
3- Create a DNP3 Direct Outstation Set- right-click where you want to create the Direct Outstation Set select DNP3 and select Direct Outstation Set.
4- You can configure the Direct Outstation Set as below:
5- Create a DNP3 Generic Direct Outstation- right-click where you want to create the outstation select DNP3, select Generic, and select Direct Outstation
6- Configure the Outstation as follows:
You can enable the unsolicited messages if needed as follows:
Publicerad för:Schneider Electric Sverige