How to eliminate historic data duplicates or errors for a point from within ViewX
DISCLAIMER

The example below is intended to demonstrate one or more features or methods and is presented as a configuration example only. Schneider Electric assumes no liability for the use or application of this example or any portion thereof.

Sometimes you may want to eliminate historic data duplicates or errors for a point. An easy way to do that from within ViewX is to create a button with a pick action method animation that will invoke the "Optimize data" method.
1- Create button on a mimic:


2- Double click on the button and select "Pick Action":


3- Select "Method" and click "Next":


4- Browse for the point object, select "Historic" as Aggregate and "Optimize data" as "Method", then click "Next":


5- Click on "Next" then "Finish" to end the configuration.

Now you can save the mimic, put the mimic in "Runtime" and click on the button. The "Optimize data" method will be triggered for that particular point.

Schneider Electric Sverige