Hur kan vi hjälpa dig idag?

Control Expert15,SP1 returns Integrity Check error.

Attempts to run Control Expert 15, SP1 after installing returns the following Integrity Check error:
c c



This can occur if there is more than one' **IntegrityCheckHash.dll' file located in the folder named 'C:\Program Files (x86)\Common Files\Schneider Electric Shared\SRCSDK'.
ccc cz



To resolve the issue, either rename the file or delete the file.
zxc