What is the function of control module ?
The control module is core of the contactor, which contains the coil assembly, diagnostic function, control terminal and PLC input terminals and PLC control (PLC control is only available in Advanced version). The coil control voltage and PLC inputs are connected to the control module. The control module also consists a LED on the front to indicate the different type of diagnosis status.