Issue:
My ATV630 drive is not responding to my 4-20 ma input.
Product Line:
ATV630
Environment:
4-20 ma input
Cause:
n/a
Resolution:
Go to Menu 5.5 ( Command and Reference) Check to see if the correct speed reference is assigned.
Then go to I/O menu and check the analog input type (current or voltage and correct min and max).
Then can go to the I/O map ( Menu 4.10) and display the analog input image to see what the drive is seeing.
Publicerad för:Schneider Electric Sverige