Hur kan vi hjälpa dig idag?

The 170ADM39030 Datasheet incorrectly shows the input and output voltages

The 170ADM39030 datasheet posted on se.com prior to March 2022 incorrectly showed the Discrete Input voltage as 20…115 VAC.
It should be, 24 VDC, (11…30 VDC).

The datasheet also incorrectly showed the Discrete Output voltage as only 20…115 VDC.
It should be, 20…115 VDC, 24…230 VAC.


This identifies where in the datasheet the corrections will be applied.

170ADM39030 datasheet corrections
Note that the User Guide shows the correct Discrete Input and Discrete Output voltages.


Schneider Electric Sverige

Utforska mer
Produkt:
Utforska mer
Produkt: