Is there a direct replacement for the XBTGH2460 HMI?
Issue:
Is there a direct replacement for the XBTGH2460 HMI?
Product Line:
XBTGH
Resolution:
Unfortunately, per our Marketing team, there will not be a replacement for the XBTGH in the future due to low sales volume.
If you are looking for an HMI with membrane keys and a touchscreen, you could look into the HMIGK line of HMIs. The HMIGK's does not have a built in estop.
One could also look into the HMIGTO line of HMIs for a full touchscreen panel without membrane keys.
Publicerad för: Schneider Electric Sverige