How can I increase the Torque on the motor, on a ATV930 drive?
Issue:
How can I increase the Torque on the motor, on a ATV930 drive?
Product Line:
ATV930
Environment:
Increase torque
Cause:
n/a
Resolution:
Go to Complete Settings
Select Motor Parameters Recheck all the motor parameters to make sure they match the motor.
Check the rating of the drive to see if you can set Dual rating to Heavy duty?
Motor Control Type- suggest to set to SVC V
Motor Data- Motor Param Choice set to Mot CoSinus, set Motor 1 Cosius Phi to ,81 ( or the
PF on the motor nameplate)
Motor Control-IR Compensation – increase as needed, to provide more torque. Slip
compensation- decrease setting, as needed.
Go back to Motor Data and select 2nd function key (Tune) and auto tune ONLY if the motor
is cold.
Publicerad för: Schneider Electric Sverige