Hur kan vi hjälpa dig idag?

How can you program a Jog function, in a ATV212 drive?

Issue:

Programming a Jog function, in a ATV212 drive.

Product Line:

ATV212

Environment:

Jog

Cause:

n/a

Resolution:

This drive does not have a jog function, in the menus. You would need to program a Preset Speed. Go to F113 (RES) and set to 6 and set SR1 to 10 ( or whatever jog speed you need?). When F and RES goes high, should run at the jog speed.