Hur kan vi hjälpa dig idag?

Does Vijeo Designer support FTPs (File Transfer Protocol Secure)?

The Latest versions of Vijeo Designer include new features to be compliant with the Cybersecurity.
The goal of this article is to inform about FTPs (File Transfer Protocol Secure) support from the version VJD 6.2 SP12.

This article is applicable to the following products:
Harmony P6, HMIGTU, HMIGTO, HMISTU, iPC, XBTGT,

This topic is related to Vijeo Designer

From Vijeo-Designer V6.2 SP12, FTPs (File Transfer Protocol Secure) has been implemented to replace FTP for Downloading, uploading and transferring data. FTPs encrypts data transmitted over network to protect the data against sniffing.
FTPs operation follows the same procedure as FTP, there are no extra and special configuration required.

Schneider Electric Sverige

Utforska mer
Produkt:
Produktfamilj
Utforska mer
Produkt: