Hur kan vi hjälpa dig idag?

Control Expert returns error 'Impossible to save DTM Catalog file'.

This can occur if there are a large number of third party DTM's installed on the PC.

To resolve the issue,
  • Uninstall the third party DTM's.
  • Start Control Expert.
  • Update the DTM catalog.
  • Open or create an application.
  • Close Control Expert.
If you need the third party DTM's for Control Expert:
  • Install only the third party DTM's that are needed for Control Expert.
  • Start Control Expert
  • Update the DTM Catalog.
If you install any third party DTM's that are not needed for Control Expert, do not update the DTM catalog when
starting Control Expert.