Hur kan vi hjälpa dig idag?

Can Modbus communication tools connect to PLC simulator instances on one PC with different PORTs

The answer is YES. Customer just needs to set the corresponding PORT number (502, 503, 504...) in the Modbus communication tool. Thanks.