Hur kan vi hjälpa dig idag?

Can custom avatars be shared with others?

Issue:
Can I share custom avatars for TeSys Island with other integrators?  Also, where are these saved?

Product Line:
TeSys Island

Environment:
All models, All versions of SoMove (and other DTM containers such as ESME, ECE...)

Cause:
Cannot find saved custom avatars via search

Resolution:
When saving custom avatars for TeSys Island, the operator will choose the avatar name.  This saved file will be in XML format and can be shared to other users for import.  File Location is shown in the below example.  Example custom avatar name 'CustomAvatarAvOneDirection'

C:\Users\USERNAME\AppData\Roaming\Schneider Electric\TeSys_Island\CustomAvatars\CustomAvatarAvOneDirection