Hur kan vi hjälpa dig idag?

Does the ATV630 and ATV930 Profibus option card VW3A3607 feature both DPV0 and DPV1?

Issue:

ATV630 Profibus option card VW3A3607 features DP and DP V1?

Product Line:

ATV630 and ATV930 Profibus option card VW3A3607 only

Environment:

All

Cause:

Features DPV0 and DPV1

Resolution:

Yes, this profibus option card VW3A3607 does support both DPV0 and DPV1