Which Lexium P Robots version are washdown and non washdown?
Only the IP class of the robot does not reveal whether it is a washable or non-washable version of the Lexium P robot, as our motors already reach IP65.
The washdown version is better/easier to clean; there are no places where water can accumulate, everything is protected by the housing (cables and motors).
Exceptions are:
- VRKP4L0RWD00000
- VRKP4L0FWD00000
These two P4 types have ILM motors with closed standard housing, therefore are washdown, too.
See also "Housing type" inside Lexium P Robot Hardware Guide.
Publicerad för: Schneider Electric Sverige