Våra varumärken

Impact-Company-Logo-English Black-01-177x54

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What lugs can I use with Altivar Process Frame Size 6 drives?
Issue:
Are there lugs available for Altivar 630 and 930 Frame Size 6 drives?

Product Line:
ATV630, ATV930

Environment:
All

Cause:
NA

Resolution:
Please see the ATV930 installation manual and ATV630 Installation manual for lug information on Size 6 drives.
The kit we recommend is "DZ2FH6" and "DZ2FH1" available on SE.com: