Security Expert, loggning av data och rensning
Security Expert har händelser och programmering lagrad i SQL databasen.
Det finns en inställning för hur länge data ska sparas vilket ställs in i Security Experts klient.
Dock kan det redan skapats större mängd data och den behöver hanteras manuellt
Vänligen läs hela beskrivningen, inklusive uppmaningen att först göra en backup!
Ytterligare kan loggning begränsas med dessa inställningar:
Reducing Unnecessary
Events By default the Security Expert system produces a large number of events that are typically not required (such as motion detection in disarmed areas). On busy sites this can quickly fill up the events database.
To reduce the number of unnecessary events, you can turn off events for inputs and outputs.
1. Navigate to Programming | Inputs.
2. Press Ctrl + A to select all inputs. 3. In the Options tab, disable Log to event buffer.
This prevents logging of open, close, tamper and short events.
The controller will still generate events for alarms, REX and other effects of the input changes.
4. Click Save.
5. If there are any inputs that require a high level of auditing, select them and re-enable Log to event buffer.
6. Navigate to Programming | Outputs.
7. Press Ctrl + A to select all outputs.
8. In the Options tab, disable Log output events. This prevents logging of on and off events.
9. Click Save.