What is the Maximum capacity of the SURT013?
Question:
What is the Maximum capacity of the SURT013 equipment cart?
Product Line:
SURT013
Environment:
Smart-UPS UPS
Solution:
The maximum recommended capacity of the SURT013 is 550Lbs based on its design. While the cart has 4 pieces of 650 lbs rated casters but we do not suggest exceeding the 550 limit. The limit takes the cart's weight and includes a safety buffer to accommodate dynamic load weight when in motion. Installing equipment that exceeds this weight may cause damage to equipment or may result to injury.
Unit is made specifically for the SURT15KRMXLT and SURT20KRMXLT using it with other equipment is not recommended.
SURT15KRMXLT and SURT20KRMXLT UPS units may be stacked to a total height of not more than 18U on its own on the floor without the cart. But when using cart only UPS and First Battery pack should be installed and additional accessories such as additional External packs , Stepdown Transformers should be installed in a separate cart.
Here are the UPS supported and Battery packs and their weight.
- SURT15KRMXLT - 546.15 lbs(US) (247.73 kg)
- SURT20KRMXLT - 546.15 lbs(US) (247.73 kg)
- SURT192RMXLBP2 - 400.84 lbs(US) (181.82 kg)
Here are some SURT15KRMXLT and SURT20KRMXLT configuration bundles that when installed Needs to be split in multiple carts because it exceeds weight capacity.
- SURT15KRMXLT-TF5 - 641.35 lbs(US) (290.91 kg)
- SURT20KRMXLT-TF5 - 641.35 lbs(US) (290.91 kg)
If you have any clarifications or concerns, please do contact us at 1-800-800-4272 or chat with our Technical Support Agents.
*Attached on this article is the user guide that shows top and bottom Image of cart and shows in detail how the UPS is mounted and installed on equipment cart.