Hur kan vi hjälpa dig idag?

PME 2024 R3 - Can´t save Registration in Web Applications

Issue:

Can´t save Registration in Web Applications


Solution / workaround


Change the way the phone number is written.


Do not use (+)


Use: ex (46) or (0046) instead of (+46)