How to determine the BOM of ATSNSX references in Singapore Pricebook
First we need to understand what the order code mean, in the Singapore Pricebook we have 3 variants
1) Source changeover composed of Switch Disconnectors
2) Source changeover composed of Breakers with identical TM-D trip unit
3) Source changeover composed of Breakers with identical Micrologic 2.3 trip unit
Source changeover composed of Switch Disconnectors
Example reference is ATSNSX010A3F, we can check on its nomenclature as per below:
Source changeover composed of Breakers with identical TM-D trip unit
Example reference is ATSNSX010B3FTM, we can check on its nomenclature as per below:
Source changeover composed of Breakers with identical Micrologic 2.3 trip unit
Example reference is ATSNSX040F3FMI2, we can check on its nomenclature as per below:
Just to take note that for remote controlled source changeover:
For ComPact NSX100 to NSX630, each circuit breaker (Normal and Replacement) must be equipped with:
- a motor mechanism
- an OF contact
- an SDE contact.
The components are supplied ready for assembly and the circuit breakers prewired. The prewiring must not be
modified.
We can then refer to photo below for typical composition of ATSNSX for 100 to 630A.
Lastly we need to use product selector to extract BOM references -> https://www.se.com/sg/en/product-range/64117711-transferpact-compact-nsx-compact-ins-inv-based/#products
Example for ATSNSX010B3FTM
BOM will be:
C10B3TM100 x 2 sets
LV429434 x 2 units
29450 x 4 units
LV429270 x 2 units
29352 x 1 unit
29349 x 1 unit
For clarifications please reach out to Customer Care Center via:
Website: https://www.se.com/sg/en/work/support/
Email: customercare.sg@schneider-electric.com
Phone: +65 6484 7877