Naše značky

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Cyber Sciences SER-3200 (Sequence of Events Recorder Event Type "Test Status Change".

Looking at the SER-3200 Web Page, you will see under Events you see that the Event Type is "Test Status Change" these events were triggered by the simulator under the control tab of the Cyber Sciences SER (Page 20 of the SER-3200 User Guide). The SER-3200 test mode simulates automatic sequencing of inputs off-to-on and back to off in 1ms intervals. Each status change is recorded as an event in the event log, along with events designating the start and end of the test mode. The test event records can be used to verify proper operation with application software.
.Cyber Sciences Recorder

NOTE: If these Input points are set to be paged on, e-mails will be sent out for each test status change. To ensure that users do not get flooded with e-mails on these events please ensure that the SER in test is placed in maintenance mode of ENM.