Naše značky

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
What terminals can the speed pot be wired to on the Altivar ATV61 and ATV71 drives?
Issue:
Terminals to connect Speed Potentiometer on ATV61/71 Drives

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to know where the Pot can be wired on the ATV61 or ATv71 drive.

Resolution:
The Pot will have 3 terminals  The center terminal is the wiper it is wired to AI1+
1st leg is wired to +10vdc
3rd leg is wired to com that is jumpered to AI-