Naše značky

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
How to display only active alarms in Vista or Diagrams for export in PME 7 & 8?
Issue
User wants a list of all current active alarms that can be exported to excel

Product
StruxureWare Power Monitoring (SPM) 7.0.x
Power Monitoring Expert (PME) 7.2.x, 8.x

Environment
Vista and Web Diagrams

Resolution

1) Open Vista and select a current diagram or create a new diagram

2) With the diagram toolbox open, drag and drop a new datalog viewer object

3) Setup the datalog viewer and edit the query and copy and paste the following query.

SELECT [SourceName]
,[SourceType]
,dbo.DateAsUnix(TimestampUTC)  AS timestamp
,[Priority]
,[Cause]
,[CauseValue]
,[Effect]
,[EffectValue]
,[AckTimeUTC]
,[AckUserName]
,[AckRemark]
FROM [ION_Data].[dbo].[vAlarmLog]
where endID is null and (not type = 0) and priority > 64
order by timestamputc desc

4) Save the diagram and open datalog viewer in Vista or web diagram

5) Copy the contents of the table to excel