Ako vám dnes môžeme pomôcť?

What is the din rail mounting kit part number for the ATV320?

Article available in these languages:

  • japončina

Issue:
Is there din rail mounting kit available for the ATV320 drive?

Product Line:
ATV320

Environment:
All

Cause:
Desire to utilize din mounting kit option

Resolution:
The mounting kit part numbers for this drive are VW3A9804 or VW3A9805.

VW3A9804 covers the following range of drives:
ATV320U02M2C
ATV320U04M2C
ATV320U06M2C
ATV320U07M2C
ATV320U02M3C
ATV320U04M3C
ATV320U06M3C
ATV320U07M3C

VW3A9805 covers the following range of drives:
ATV320U11M2C
ATV320U15M2C
ATV320U22M2C
ATV320U11M3C
ATV320U15M3C
ATV320U22M3C
ATV302U04N4C
ATV320U06N4C
ATV320U07N4C
ATV320U11N4C
ATV320U15N4C
ATV320U07S6C
ATV320U15S6C

Note: The din rail mounting kits are only available for the above drives. The other drives not list above do not have a din rail kit.