Naše značky

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
What are the hardware and software requirements for Vijeo Designer v6.2?
Issue:
What are the hardware and software requirements for Vijeo Designer v6.2?

Product Line:
VJD, Vijeo Designer

Resolution:

The following table lists the system requirements for the Vijeo Designer Editor.

Requirement

Vijeo Designer Editor

Platform

PC

CPU

Pentium 4 - 2 GHz or faster recommended

Memory

1 GB minimum, 2 GB or more recommended

Available Disk Space

2.0 GB or more on hard disk

Operating System

Microsoft Windows XP Professional (Service Pack 3 or higher)

Microsoft Windows 7 32 and 64 bit

Microsoft Windows 8.1 32 and 64 bit

Microsoft Windows 10 32 and 64 bit

Web Browser

Microsoft Internet Explorer 6.0 (Version 7 or higher recommended)