Naše značky

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
What can cause an INF6 fault on the ATV320 Drives?
Issue:
INF6 fault on ATV320

Product Line:
ATV320 drives

Environment:
All

Cause:
The option installed in the drive is not recognized.

Resolution:
• Check the reference and compatibility of the option.
• Check that the option is well inserted into the ATV320.