Naše značky

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Power Monitoring Expert v2020: Error while launching PME thick applications (Management Console/Vista/Designer)

Issue
In few sites after successful installation of PME v2020 it was observed below errors while launching PME thick applications like Management Console, Vista and Designer.
a

Environment
Power Monitoring Expert v2020

Cause
The issue is due to LAN proxy server settings blocking connection to local address (localhost).

Resolution
To fix this issue either
> Disable Proxy server.
or
> Enable the bypass proxy server for local address.

This setting is accessible by opening Internet Explorer > Tools > Internet Options > Connections > LAN Settings > Proxy Server
b