Naše značky

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
video: How to reduce Harmonics with passive filter and set iFi [Input Filter] function on ATV600, ATV900 ?

🎥 Looking to learn more about harmonic reduction and configuring the iFi function?

In this video, dive into the realm of passive filters and discover how they can help mitigate unwanted harmonics.

We'll also provide an in-depth explanation of configuring the iFi function to optimize its usage.



🔔 Timestamps:
0:13 - Introduction
0:38 - Harmonics and Altivar Process Drives
1:27 - Passive filter
3:07 - Connection with shunt
3:37 - Connection with contactor
4:39 - General Programming
6:22 - Importance of using [Input Filter] iFi parameter

➡️For more information see:
● Catalog for Altivar Process ATV600: DIA2ED2140502EN
● Catalog for Altivar Process ATV900: DIA2ED2150601EN
● ATV630-650 Installation manual: EAV64301
● ATV930-950 Installation manual: NHA80932
● Instruction sheet - ATV Passive Filters - VW3A46101 ... A46176 : EAV38321
● Instruction Sheet: Passive filters - VW3A46101A ... VW3A46116A: NHA88101
● Instruction Sheet: Passive filter VW3A46117A : NNZ63894
● Instruction Sheet - Passive filters VWA346118A...VW3A46121A: NNZ37670
● Instruction Sheet: Passive Filters VW3A46122A...VW3A46181A: BQT77693