Naše značky

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
Can you change or add a new username with the cyber security feature on the ATS480 Soft Starter?

Issue:

Changing or adding a new username when connecting with Ethernet on the ATS480 Soft Starter

Product Line:

ATS480 Soft Starter

Environment:

All

Cause:

Cyber Security feature

Resolution:

No, you cannot currently add a new username or change the username from ADMIN. You can only change the password or deactivate the cyber security feature.