Naše značky

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
		
Ako vám dnes môžeme pomôcť?
ETE - FAQ - Transformer: How do water and oxygen levels shorten the life of paper insulation?

Oxygen and water both have a substantial impact on the life of the insulation. These oil pollutants interact to breakdown the polymer chains of the insulation paper. As these chains get smaller the paper becomes brittle and cracks occur. Breakdown can occur in these cracks resulting in catastrophic damage.